(!)Due to Microsoft's end of support for Internet Explorer 11 on 15/06/2022, this site does not support the recommended environment.

Misumi Threading Cutter Product CNC Program Download Services

Image

You can download Misumi threading cutter CNC programs (G codes) for each product as Excel files. * Note: As programs may not operate depending on security levels, confirm Excel settings in advance.

Created as a Microsoft Excel 97-2003 worksheet (.xls).

Excel Download

Security Settings Procedure for Misumi Threading Cutter CNC Programs

Please note that we assume no responsibility for any damage resulting from use of the Misumi Threading Cutter CNC Programs or from macro security setting changes intended for their use.

Security Settings Procedure for Threading Cutter CNC Programs (PDF/685 KB)

How to Use CNC Programs

  1. STEP 1 In the "List" sheet, select and click on the model number of the tool to be used. (Transfers to "InputPara" sheet)
  2. STEP 2 Select the processing size and press the "Change" button. The selected tool dimensions are reflected in the cutting conditions input table at the bottom of the sheet.
  3. STEP 3 Next, click on the illustration of the processing direction to be used.
  4. STEP 4 Enter values into the yellow field of the cutting conditions input
  5. STEP 5 Press the "Automatic Calculation" button.
  6. STEP 6 G codes are displayed for Absolute (Main) and Incremental (Sub). Press the "Export File" button to download each G code as a text file.

Excel Download

Security Settings Procedure for Misumi Threading Cutter CNC Programs