(!)Due to Microsoft's end of support for Internet Explorer 11 on 15/06/2022, this site does not support the recommended environment.
A wide variety of standard and configurable components for factory automation engineers in industries such as automotive, semiconductor, packaging, medical and many more.
A good selection of accessories such as screws, bolts, washers and nuts that you may need for your daily engineering usage.
Browse industrial materials ranging from heat insulating plates, sponges, to metal and plastic materials in different sizes to meet your various applications.
A wide variety of wiring parts for connecting and protecting control and PC parts including Connectors, Cables, Electric Wires, Crimping Terminals and more.
A wide variety of controls and PC parts for electrical engineers including Controls, Powers, PC parts and more.
A wide variety of cutting tools for many uses and work materials including End Mills, Drills, Cutters, Reamers, Turning Tools and more.
A wide variety of tools and supplies used in processing including Machine Tools, Measurement Tools, Grinding and Polishing Supplies and more.
A wide variety of goods used in shipment, material handling and warehouse including Tape supplies, Stretch film, Truck, Shelf, Crane and more.
A large variety of goods for every kind of factories and offices including Protection items, Cleaning supplies, sanitations, office supplies and more.
A large variety of items used in R&D and Clean Room including research Equipment, Laboratory Essentials, Analysis Supplies, Clean Environment-Related Equipment and more.
Choose from thousands of standard stamping die components including Punch & Die, Gas Springs, Guide Components, Coil Springs and many more.
Browse our wide variety of mold components including Ejector Pins, Sleeves, Leader Components, Sprue Bushings and many more.
Browse our injection molding components including Heating Items, Couplers, Hoses and more.
This translation is a Google translation Terjemahan ini adalah terjemahan Google
Timing Belt and Pulley Image from Photomacrography
MISUMI have been contacted by customers for question below :
Q : "Dear MISUMI Technical Support Team,
We are building a machine that has several shafts driven by stepper motors. These shafts need to be synchronized to each other, but at different speeds. We did some research and it looks like a timing belt system will solve our problem, but we don’t know how to proceed with selecting parts. Could you please provide some tips or recommendations?"
MISUMI is always happy to give advice on various products for machines that need to work in relation to the various parts.
A: With any synchronization project, it’s all about the timing. Let’s start with a brief introduction on timing belts, pulleys, and how they work together
A timing belt is used when the rotation of two different shafts need to be exactly linked. Normal power transmission belts and pulleys are smooth, so the belt can occasionally slip off track (one shaft would be turning while the other remains still). On the other hand, timing belts and pulleys have teeth, which lock the rotation of the shafts and prevent misalignment. In a car, the timing belt links the engine crankshaft to the valve camshaft, thereby making sure that the valves open and close at the correct times. If that belt tears or breaks a tooth, the valves can open at the wrong time and ruin the engine.
There are a lot of different variables for belt sizing – width, number of teeth (pitch), material, etc. Each manufacturer will have different recommendations based on your project’s specifications, taking into account shaft speeds, power transmission, environment, and other concerns. Take care not to needlessly oversize – a larger, stiffer belt can cause difficulties with smaller drive motors.
As with any belt and pulley system, you need to identify the rotation ratio between the shafts. For instance, if shaft #1 needs to spin twice as fast as shaft #2, you would have a 2:1 ratio. Once this ratio is calculated, you can then select the pulleys. Looking at the number of teeth on the pulley, find two that match your desired ratio. Continuing with our example, if we had a 16-tooth pulley on shaft #1, we would need a 32-tooth pulley on shaft #2.
Figure showing belt length from Nonstop Systems
The next tricky part of the design is figuring out the belt length. You need to know the distance between the centers of the two shafts and the pitch diameters of the two pulleys, which is usually specified by the manufacturer. Most belt manufacturers will provide an online calculator for finding lengths of their belts, but the following formulas can be used to calculate belt length:
If you need an exact measurement, you can use the following formula:
where:
Note that these formulas don’t take into consideration any pretension on the belt – most recommendations are for 1% – 8%. Belts are only made in certain lengths, so you may need to slightly adjust shaft spacing or pulley diameters to find one that works for you.
Now, all of your system components should be in place. We’ve identified the proper belt type based on the system requirements and manufacturer recommendations, sized the pulleys to the correct shaft ratio, and calculated the belt length.
Put everything together, and you’ve got a fine tuned machine which work perfectly.
270H075G
60S3M1050G
30T8012.7
100S2M80G
HTBO-S5M250-500
HTBN1000S5M-100
TBCR-S5M150
TTBU1000T10-250
Have you ever got a problem with ordering? Click here and let us help you!